Topic: System Upgrade

Transitioning to MDrivePlus Motion Control from Legacy MDrive

The MDrivePlus Motion Control products represent significant improvements over the legacy MDrives. Based on new patented technology, they feature a richer software command set, improved current control, and enhanced thermal dissipation. Along with these improvements, there may be situations where the MDrivePlus are not “drop-in replacements” for existing legacy MDrives. Some customers may have software …

Transitioning to MDrivePlus Motion Control from Legacy MDrive Read More »

Transitioning from MicroLYNX

Hardware differences These two systems have very different hardware features and functions. For example, the MicroLYNX has expansion slots, and the MForce does not. These slots allow up to a total of 24 isolated digital IO. In the MForce Plus^2 version, there are eight digital 5-24 VDC IO which are non-isolated. Hardware features not available …

Transitioning from MicroLYNX Read More »

Upgrading CANopen Bootloader & Firmware

The boot loader version is located in the product identification block at the right of the home screen of the CANopen Configuration utility. SEM recommends using the latest firmware and boot versions. Requirements: Lexium MDrive Software Suite with the CANopen Configuration Utility installed. The latest firmware and bootloader files for the Lexium MDrive CANopen products, …

Upgrading CANopen Bootloader & Firmware Read More »

Transitioning from IMx products

Transitioning from IM483/IM805 to MForce Step/direction When converting an application from IM483/IM805 drives to MForce Step and Direction drives, there are many considerations. These two systems have very similar stepper drive capabilities. The MForce’s current capability is listed in RMS Amps while the IM483/IM805 drives output currents were listed in Peak Amps. As a result, …

Transitioning from IMx products Read More »