Menu

Topic: Programmable I/O

MCode: Programming MDrive I/O

Global or Local variables Like All MDrive variables, the I/O point configuration can be declared two ways: Globally Locally Global:  Global I/O configurations, are declared outside the main body of the program. These are more typical and are used when you want the I/O point to have the same function at all times. Local:  Local …

MCode: Programming MDrive I/O Read More »

Move on BCD

 

Multiple Position Trips

Lexium MCodeMDrive MCode    

Electronic Gearing

 

Do NOT follow this link or you will be banned from the site!