Topic: Networking

Serial RS-422/485 wiring

Lexium MDriveMDrive Single interface Wiring diagram:  Full duplex (4-wire) only Figure 1: Single Lexium MDrive full duplex point-to-point configuration  Notes and checkpoints Ensure the crossover between the interface and Lexium MDrive (Rx—Tx / Tx—Rx) Ensure the crossover between the interface and Lexium MDrive (Rx—Tx / Tx—Rx) Ground is galvanically isolated on the Lexium MDrive If …

Serial RS-422/485 wiring Read More »