Topic: Motion

First program: programming motion

Program flow The flowchart below gives a functional overview of what processes the program will employ. The short overview is that the program will ask for some rotations, ask an axis direction, and then perform the move. Once motion is complete, the axis position will be displayed, and the program will ask to repeat or …

First program: programming motion Read More »

Multiple Position Trips

Lexium MCodeMDrive MCode    

Electronic Gearing

 

Basic Motion Sample

 

Move on Analog Input

 

Turn Table

 

Basic Motion Sample