Topic: Modbus/TCP

Modbus/TCP vs MCode/TCP Overview

MODBUS/TCP (Connect to port 502) MODBUS/TCP is a standard protocol designed for multidrop networks based on a client-server architecture communicating over TCP/IP. MCode/TCP (Connect to port 503) MCode/TCP is a protocol based upon the MDrive programming language using 1 and two character mnemonics. Depending on the port selected (ip.address:502 or ip.address:503) the device operation will …

Modbus/TCP vs MCode/TCP Overview Read More »

Connecting a Maple Systems HMI

Lexium MDrive Setup Locate the Lexium MDrive Software Suite for download at the below link: https://motion.schneider-electric.com/lmd/lexium-mdrive-software.php Once installed on your PC, open the Lexium MDrive Software Suite and select “Install Lexium MDrive Ethernet Interface”. This will install the TCP/IP utility within the Lexium MDrive Software Suite for use. After installing this utility, a green check …

Connecting a Maple Systems HMI Read More »

Connecting a Proface HMI

Lexium MDrive Setup Locate the Lexium MDrive Software Suite for download at the below link: https://motion.schneider-electric.com/lmd/lexium-mdrive-software.php Once installed on your PC, open the Lexium MDrive Software Suite and select “Install Lexium MDrive Ethernet Interface”. This will install the TCP/IP utility within the Lexium MDrive Software Suite for use. After installing this utility, a green check …

Connecting a Proface HMI Read More »