Topic: Ethernet TCP/IP

Modbus/TCP vs MCode/TCP Overview

MODBUS/TCP (Connect to port 502) MODBUS/TCP is a standard protocol designed for multidrop networks based on a client-server architecture communicating over TCP/IP. MCode/TCP (Connect to port 503) MCode/TCP is a protocol based upon the MDrive programming language using 1 and two character mnemonics. Depending on the port selected (ip.address:502 or ip.address:503) the device operation will …

Modbus/TCP vs MCode/TCP Overview Read More »

Ethernet upgrade failure

Enable Telnet Client In order to recover the MDrive or LMD from this state you will need to enable your “Telnet Client” on your computer. By default, with Windows based systems, this client is disabled. Open the Widows Control Panel Select “Programs and Features”: Once in “Programs and Features”, select “Turn Windows features on or …

Ethernet upgrade failure Read More »

Windows Firewall Configuration

Configure Windows Firewall to unblock UDP Port 69 Create an Inbound Rule Open the Windows Control Panel Open Windows Firewall Click “Advanced Settings.” On the Advanced Settings screen, select “Inbound Rules.” On the right column of the screen, select “New Rule.” The New Inbound Rule Wizard dialog will open. Select the radio selector labeled “Port” …

Windows Firewall Configuration Read More »

Connecting a Maple Systems HMI

Lexium MDrive Setup Locate the Lexium MDrive Software Suite for download at the below link: https://motion.schneider-electric.com/lmd/lexium-mdrive-software.php Once installed on your PC, open the Lexium MDrive Software Suite and select “Install Lexium MDrive Ethernet Interface”. This will install the TCP/IP utility within the Lexium MDrive Software Suite for use. After installing this utility, a green check …

Connecting a Maple Systems HMI Read More »