Home > Resources > Lexium MDrive Linear Actuator

Lexium MDrive Linear Actuator

Select from the available features to build the for the desired Lexium MDrive integrated stepper motor linear actuator product and lead screw characteristics.

Part Number:

Select from the available options to build a part number.






Screw Selection







Connectivity Accessories

Accessory Function Part Number
Misc Accessory
Communications Converter
Prototype Develoment Cable(s) Signal Cable
Power Cable
Communications Cable
Connector Kit(s)
(only needed for replacements)
Pluggable, set of 3