Home > Resources > Lexium MDrive Electric Cylinder part builder

Lexium MDrive Electric Cylinder part builder

Select from the available features to build the for the desired Lexium MDrive integrated stepper motor electric cylinder products.

Part Number:






*


Stroke length is measured in inches and is available in 0.1 inch increments

Product

Communications Interface
Feedback
Protocol
Input Voltage
Connector Style
IP Rating

Cylinder Details

Load Limit lbs (kg)
Stroke Length inches (cm)
(
)
Nut Type
Mounting
Stack Length