Menu

Product Family: Motion, Drives & Controllers

HY462-CN021 21 Pin Right Angle Connector

HY462-CN021 21 pin right angle connector for the IB462He PCB-mount driver module mounts to the user’s PCB prior to soldering to provide an easy pluggable interface for the driver module.

H-462H Heat Sink

Heat sink for the IB462He PCB-mount driver module. Includes mounting hardware.

Do NOT follow this link or you will be banned from the site!