Menu

Product Family: MDrive Linear Actuator

Setting up your Ethernet adapter for MDrive Ethernet TCP/IP products

[vc_row][vc_column][vc_column_text][/vc_column_text][vc_column_text] Step-by-step: setting up your PC Ensure your computer “Local Area Connection” port matches the IP Address structure of the motor you wish to upgrade. All Lexium MDrive motors ship from the factory at a default of 192.168.33.1. If you need assistance in setting up your IP settings to be able to communicate continue reading …

Setting up your Ethernet adapter for MDrive Ethernet TCP/IP products Read More »

CANopen – Profile position mode

The below example sets typical motion profile commands a system would configure1, enabling the motor power2 and the four different move types3supported in Profile Position Mode using SDOs with Node ID 41h. 1Typical motion profile commands could be set each time on power up from host or set using a configuration file and stored to …

CANopen – Profile position mode Read More »

Do NOT follow this link or you will be banned from the site!