Menu

Product Family: Lexium MDrive Linears

Upgrading the Lexium MDrive Ethernet TCP/IP Application Firmware

Before you begin This upgrade procedure is for Lexium MDrive models with a Kinetis K64 processor using the 2.4.x.x firmware. The following prerequisite steps are required before performing a firmware upgrade on your Lexium MDrive Ethernet TCP/IP product. Download and install the Lexium MDrive Software Suite. Download and extract the Ethernet Application Firmware file. From …

Upgrading the Lexium MDrive Ethernet TCP/IP Application Firmware Read More »

Do NOT follow this link or you will be banned from the site!