Home > News > Press Releases > More Than One Million MDrive® Integrated Motors Sold
More Than One Million MDrive® Integrated Motors Sold
Over 1 million MDrive® integrated motors have sold since 2001
Marlborough/CT, November 19, 2019 — Over 1 million MDrive® integrated motors have sold since 2001 when they revolutionized motion system design by replacing multiple separate components with one compact all-in-one motor and electronics package. MDrive products pioneered the marriage of motor and electronic components all in one compact package, leading to the birth of today’s motion industry staple: integrated motors.
Integrated motors can simplify motion system design. Their all-in-one design of motor and electronics has vast advantages in today’s fast-paced industrial environment. “With an integrated motion solution, when you mount the motor you’ve also mounted the electronics which are prewired onto the motor,” according to Russ Gibas, Manager of the R&D group that developed MDrive. “With the addition of power, you can basically plug in and go.”
Since its initial launch almost 20 years ago, the MDrive integrated motor family has moved stepper motion control technology to a new level, increasing accuracy while providing additional benefits in a compact package. What began with reducing the electronics package size to fit onto a stepper motor using surface-mount technology and application specific integrated circuits (ASICs), has expanded to include features previously unavailable on stepper motors. The latest MDrive products offer closed-loop performance, velocity control, energy savings, and a range of standardized communication choices including EthernetTCP/IP and CANopen. Numerous options and accessories are also available including absolute encoder, captive shaft electric cylinder, gearboxes and more.
With all-in-one, integrated motion control solutions such as MDrive products, a machine’s complexity, size & cost can be greatly reduced. What in the 1970s was a phone-booth-sized rack-mount enclosure containing a manually programmed drive, has evolved to a complete programmable motion control system integrated onto a motor.
MDrive products are assembled in our USA factory, which is certified ISO9001:2015 and ISO14001:2015: https://motion.schneider-electric.com/dloads/certificationssustainability/. Built to order, products are available with a wide range of standard features. For applications requiring something unique, our FlexCenter is dedicated to finding custom solutions. Use the inquiry form https://motion.schneider-electric.com/all-products/custom-products/ to begin a discussion.
More product information is available at https://motion.schneider-electric.com/all-products/
To locate a distributor in your area, go to https://motion.schneider-electric.com/contacts/
About Schneider Electric Motion USA
SEM USA [formerly IMS] is a division of Schneider Electric, a global specialist in energy management and automation, with 170,000 employees serving customers in over 100 countries, helping them to manage their energy and process in ways that are safe, reliable, efficient and sustainable. www.motion.schneider-electric.com
When it comes to your form, fit and function requirements, don’t settle. Get precisely what you need working with us. We know motion.
Contact us with any questions about how we can help you with your motion application or for assistance with your SEM products.
Browse our resource section and find the most useful tools and documents for all our products.