Variable Reluctance Motors have no permanent magnet, thus the rotor spins freely as there is no detent torque. The step angle of a VR motor is in the medium range, generally 5 to 15 degrees. This type of motor is also used in non-industrial applications where a high degree of torque is not required.