These motors are composed of two windings, each with a center tap. The center taps are either brought outside the motor as two separate wires or connected to each other internally and brought outside the motor as one wire, resulting in 5 or 6 wires.