Control Area Network (CAN)

Is a serial bus system, which was originally developed for automotive applications in the early 1980’s. The CAN protocol was internationally standardized in 1993 as ISO 11898-1 and comprise the data link layer of the seven layer ISO/OSI reference model.