Bipolar Motors

These motors are composed of two windings and have four wires with no center taps. Current flow is bidirectional and runs through an entire winding at a time instead of just half of the winding. As a result, bipolar motors produce more torque than unipolar motors of the same size.