Ballscrew

Ballscrews are highly efficient low friction and low backlash lead screw devices that use ball bearings rolling in a channel cut into the screw. The low friction and backlash attributes are extremely valuable for precision applications where they are used to driver the axes of the machine.