Closed loop on error

Example Program

Closed loop on error

Description

This program illustrates closed loop control with an On Error (OE) routine which will perform math functions on the counters to display the position error.

The code shown on the right may be copied and pasted into the program editor window of the Motion Control Programmer application, or a zip file containing the program files may be downloaded below.

Topics

  • Closed Loop/Encoder
  • MCode OS

Applicable Product

  • Lexium MDrive
  • MDrive Linear Actuator
  • MDrive Plus
  • MForce

Resource Files

Rc=80 Mt=50 'enable encoder functions, configure stall settings Ee=1 Sf=15 Sm=0 'motion variables are scaled 'to encoder counts instead of microsteps A=20000 D=A Vi=2048 Vm=15000 'user variable created to hold move count VA Q1 '[PROGRAMS] 'program block Ga sets the on 'error handle routine to call K1 PG 1 LB Ga OE K1 P=0 'program block Gb contains the 'motion loop which will run 100 times LB Gb MR 51200 H H 500 MR -51200 H H 500 IC Q1 BR Gb,Q1<100 CL K1 E '[SUBROUTINES] 'Subroutine K1 sets the response 'for the on-error handler. It will 'perform some math to determine the 'position error in encoder counts, 'as well as display the error # if 'one occurs. LB K1 R3=C1/25 R1=R3 - C2 PR "Counts error = ",R1 PR "Error = ",Er Er=0 H 20 RT PG S 'Keep this line to save program on load '[END]
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
'LEXIUM MDRIVE DEMO PROGRAM
'Last modified 02/21/2013
'Sample test program for demonstration purposes only
'Not tested or verified for safety or any function
 
'[VARIABLES]
Rc=80
Mt=50
 
'enable encoder functions, configure stall settings
Ee=1
Sf=15
Sm=0
 
'motion variables are scaled
'to encoder counts instead of microsteps
A=20000
D=A
Vi=2048
Vm=15000
'user variable created to hold move count
VA Q1
 
'[PROGRAMS]
'program block Ga sets the on
'error handle routine to call K1
PG 1
  LB Ga
      OE K1
      P=0
      
    'program block Gb contains the
    'motion loop which will run 100 times  
  LB Gb
      MR 51200
      H
      H 500
      MR -51200
      H
      H 500
      IC Q1
      BR Gb,Q1<100
      CL K1
    E
  
  '[SUBROUTINES]
  'Subroutine K1 sets the response
  'for the on-error handler. It will
  'perform some math to determine the
  'position error in encoder counts,
  'as well as display the error # if
  'one occurs.
  LB K1
      R3=C1/25
      R1=R3 - C2
      PR "Counts error = ",R1
      PR "Error = ",Er
      Er=0
      H 20
      RT
  
  PG
S
'Keep this line to save program on load
'[END]