Basic Motion Sample

Example Program

Basic Motion Sample

Description

This program is a very basic motion sample which makes a basic point-to-point relative move. The program will function the same regardless of the MCode product used.

Topics

  • MCode OS
  • Motion

Applicable Product

  • Lexium MDrive
  • MDrive Linear Actuator
  • MDrive Plus
  • MForce
  • Motion, Drives & Controllers

Resource Files

[wpdm_package id=8481 template=[wpdm_package id=8482 template=[wpdm_package id=6010 template=[wpdm_package id=2520 template=

Program Example