Menu

Driver-Product: MForce

MFM5 MicroDrive Step/direction Input

MForce MicroDrive Step/direction Input differential inputs is a high performance, high resolution microstepping driver. High VDC input voltage and an output current of   Parameters are set over SPI using an included utility .

MFM5 PowerDrive Step/direction Input

MForce PowerDrive Step/direction Input with differential inputs is a high performance, high resolution microstepping driver. High VDC input voltage and an output current of   Parameters are set over SPI using an included utility .

MFM1 PowerDrive Step/direction Input

MForce PowerDrive Step/direction Input with isolated +5 to +24 V universal inputs cis a high performance, high resolution microstepping driver. High VDC input voltage and an output current of   Parameters are set over SPI using an included utility .

MFM1 MicroDrive Step/direction Input

MForce MicroDrive Step/direction Input with isolated +5 to +24 V universal inputs cis a high performance, high resolution microstepping driver. High VDC input voltage and an output current of   Parameters are set over SPI using an included utility .

MFI3 MicroDrive CANopen

MForce PowerDrive CANopen with expanded d features combines a CANopen motion controller supporting DS301 and DSP402 profiles with a high-resolution microstepping drive. High VDC input voltage and an output current of   Commissioning is accomplished using a free software interface or by using CAN in Automation standard Layer Setting Services (LSS).

MFI3 PowerDrive CANopen

MForce PowerDrive CANopen combines a CANopen motion controller supporting DS301 and DSP402 profiles with a high-resolution microstepping drive. High VDC input voltage and an output current of   Commissioning is accomplished using a free software interface or by using CAN in Automation standard Layer Setting Services (LSS).

MFI1 MicroDrive CANopen

MForce MicrodDrive CANopen with standard features combines a CANopen motion controller supporting DS301 and DSP402 profiles with a high-resolution microstepping drive. High VDC input voltage and an output current of   Commissioning is accomplished using a free software interface or by using CAN in Automation standard Layer Setting Services (LSS).

MFI3 MicroDrive Programmable Motion Control

MForce MicroDrive Motion Control with expanded features combines a programmable motion controller with step and direction microstepping drive. Programming is accomplished over RS-422/485 with provided software for point-to-point or multiple unit configurations. VDC input voltage and an output current of   Fully programmable using the powerful and feature rich MCode OS.

MFI3 PowerDrive Programmable Motion Control

MForce PowerDrive Motion Control combines a programmable motion controller with step and direction microstepping drive. Programming is accomplished over RS-422/485 with provided software for point-to-point or multiple unit configurations. VDC input voltage and an output current of   Fully programmable using the powerful and feature rich MCode OS.

MFI1 MicroDrive Programmable Motion Control

MForce MicroDrive Motion Control with standard features combines a programmable motion controller with step and direction microstepping drive. Programming is accomplished over RS-422/485 with provided software for point-to-point or multiple unit configurations. VDC input voltage and an output current of   Fully programmable using the powerful and feature rich MCode OS.

Do NOT follow this link or you will be banned from the site!