Cable Drivers
MD-CC404-000 & MD-CC405-000
The MD-CC404/5-000 drivers are applicable to Lexium MDrive RS-422/485 products. This device is “plug-n-play” and the drivers should automatically install to an Internet connected PC. Should your network block automated driver installs or the PC not be connected, the drivers may be downloaded from:
MD-CC404-000 Drivers (FTDI VCP Drivers)
Note: This link will open in a new browser tab/window.
MD-CC40x-001
The MD-CC40x-001 drivers are applicable to MDrivePlus and MForce Motion Control RS-422/485 products. This device is “plug-n-play” and the drivers should automatically install to an Internet connected PC. Should your network block automated driver installs or the PC not be connected, the drivers may be downloaded from:
MD-CC40x-001 Drivers (Silicon Labs CP210x USB to UART Bridge VCP)
Note: This link will open in a new browser tab/window.
Legacy MD-CC40x-001 drivers
Use ONLY with CC4 cables with the IMS ID on 32 bit Windows systems
MD-CC50x-001
These drivers apply to the MD-CC500-000 (MDrivePlus and MForce products) and MD-CC501-000 (Lexium MDrive products) USB to CANopen Communications converters
MD-CC50x-000 Drivers (PEAK Systems PCAN-USB)
Note: This link will open in a new browser tab/window.
MD-CC30x-001
The MD-CC30x-001 drivers are applicable to MDrivePlus and MForce Step/direction and Speed Control SPI products. This device is “plug-n-play” and the drivers should automatically install to an Internet connected PC. Should your network block automated driver installs or the PC not be connected, the drivers may be downloaded from:
MD-CC30x-001 Drivers (Silicon Labs CP210x USB to UART Bridge VCP)
Note: This link will open in a new browser tab/window.
Legacy MD-CC30x-001 drivers
Use ONLY with CC3 cables with the IMS ID on 32 bit Windows systems
When it comes to your form, fit and function requirements, don’t settle. Get precisely what you need working with us. We know motion.
Contact us with any questions about how we can help you with your motion application or for assistance with your SEM products.
Browse our resource section and find the most useful tools and documents for all our products.