Content Type: Application Note

Transitioning to MDrivePlus Motion Control from Legacy MDrive

The MDrivePlus Motion Control products represent significant improvements over the legacy MDrives. Based on new patented technology, they feature a richer software command set, improved current control, and enhanced thermal dissipation. Along with these improvements, there may be situations where the MDrivePlus are not “drop-in replacements” for existing legacy MDrives. Some customers may have software …

Transitioning to MDrivePlus Motion Control from Legacy MDrive Read More »

Selecting stepper motor stack size

The capabilities of the different stack length motors are often confusing to people specifying them and designing them into systems.  The best way to think of the capabilities of the different stack lengths of a particular frame size is to think of the trade-offs.  The smaller MDrive stack length has lower torque that persists to …

Selecting stepper motor stack size Read More »