Blog: Products

Industrial connectivity and IEC61076-2-101: M12 Lexium MDrive introduced

Since the early 1990s, the Fieldbus protocols have become the preferred industrial network system for distributed control. Machines designed around these standardized networks have evolved to become more robust and environmentally resilient to meet demanding applications of ever increasing complexity.

Tale of two demos

There are two motion demos on display in the Schneider Electric Motion USA booth (S-663) at Pack Expo in Chicago, IL from October 28 through October 31, 2012. These demos are built around the new MDrive Ethernet integrated motor, drive, controller products. These demos illustrate the ability of the MDrive Ethernet products to integrate seamlessly …

Tale of two demos Read More »

MDrive EtherNet/IP integrated all-in-one motion systems for industrial automation

Video of North American Sales Manager Paul Kling discussing MDrive EtherNet/IP at MD&M West. MDrive EtherNet/IP motion systems feature integrated motor, drive and programmable I/O with standardized IP addressing, eliminating complicated wiring and programming of traditional multi-drop systems with RS-485 communications. These compact, low-cost products are ODVA conformance tested and will interface with many manufacturer …

MDrive EtherNet/IP integrated all-in-one motion systems for industrial automation Read More »