Menu

Blog: Motion System Design

ACME Screw Linear Actuator Motors

ACME screws – a cost effective alternative to ball screws

In our last posting, we talked about the positional accuracy of a point of the moveable plate or work surface of our ball screw table with the terms roll, pitch, and yaw. The application that you’re trying to solve should be with the most cost-effective positioning solution.

Linear Systems: Bearing Supports and End Fixity

Let’s start this discussion with the bearing supports for the ball screw. Let’s assume we have a ball screw that is 18” long and it provides 12” of travel. We have 3” on both ends that have been machined down past the root of the thread to form a smooth surface to install bearings that will support the screw. Let’s place the screw so it’s oriented left to right and our stepper motor and its coupling is on the left. We could install a number of bearing combinations on both ends of the ball screw that’s easier to define with a table:

Linear Systems: Thread precision and mechanical backlash

In our last posting, we introduced leadscrews, ball screws and linear slides. We’re going to continue with that discussion by considering how accurately the threads are cut into the screw. Using the five-pitch screw as an example, we understand that five revolutions are supposed to move the plate one inch, but what happens if the thread is cut too long or too short. Five revolutions might move the plate 0.990” or 1.010”.

Linear Systems: Lead screws, Ball screws and Linear Slides

With this posting, we’ll begin a discussion about leadscrew/ball screw/linear slide systems. Picture a screw with a nut on it. No, no not a Walnut.  Sighhhh. OK then, picture a right-hand threaded 1/4-20 screw with a 1/4-20 nut threaded on to the screw. A 1/4-20 screw has an outside diameter or major diameter of 0.25” and the thread of the screw has 20 turns per inch.

Fundamentals of Motion Control

[vc_row][vc_column][vc_column_text]Recently I came across a simple infographic from Power Jack Motion that did a nice job of visualizing the difference between alternating current (ac) and direct current (dc) motors. This article will follow and present the information contained therein. What is Motion Control, Anyway? Motion Control is a sub-field of automation encompassing the systems or …

Fundamentals of Motion Control Read More »

Do NOT follow this link or you will be banned from the site!