Application note

Initial Setup and Reset of CyberSecurity

Home > Resources > Application notes > Initial Setup and Reset of CyberSecurity

Description

This tutorial provides information on the initial setup of the “CyberSecurity feature” on the Lexium MDrive (LMD) standard and high-torque ethernet devices that are shipped with cybersecurity enabled.

LMD ethernet devices with a CSE mark on the product label of the motor indicates that cybersecurity is enabled on the device and additional setup is required before the device
can be used.

Applicable

  • Lexium MDrive
  • Lexium MDrive Linears

Requirements

  1. Lexium MDrive Software Suite
    (installed).
  2. IBM compatible PC running
    Microsoft® Windows 7
    or higher with available USB port
    and USB to RJ45 convertor, or
    integral RJ45 connection.

Details

Before you begin

Download and install the Lexium Software Suite.

Step-by-step for initial setup:

  1. Launch the Lexium Software Suite.
  2. Launch the Ethernet Interface from the Lexium Software Suite Launch Screen.
  3. Connect the LMD to the computer.
  4. Establish a connection through the ethernet interface using the Connect button on the Ethernet Interface.
  5. Follow the prompts to setup an ethernet password.

For information on initial setup and password reset, refer to the Setup Notes available for download from:
Initial Setup and Reset of Cybersecurity

For additional information on CyberSecurity, refer to:
Cybersecurity

Resource files

When it comes to your form, fit and function requirements, don’t settle. Get precisely what you need working with us. We know motion.

Contact us with any questions about how we can help you with your motion application or for assistance with your SEM products.

Browse our resource section and find the most useful tools and documents for all our products.