Application note
MCode: Programming MDrive I/O
Home > Resources > Application notes > MCode: Programming MDrive I/O
Description
This Application Note covers the topic of writing MDrive MCode programs using the programmable I/O points both as a single I/O point, or as a bank of 4 I/O points as a group.
Applicable
- MDrive Linear Actuator
- MDrive Plus
- MForce
Requirements
- Optional: +5 to +34 VDC Auxiliary supply
- +5 to +24 VDC I/O supply (if using sourcing outputs).
- Input and/or output devices
- Cabling: 22 AWG shielded twisted pairs for I/O, Shielded twisted pair for power, AWG determined by length and current.
Details
Global or Local variables
Like All MDrive variables, the I/O point configuration can be declared two ways:
- Globally
- Locally
Global: Global I/O configurations, are declared outside the main body of the program. These are more typical and are used when you want the I/O point to have the same function at all times.
Local: Local configurations are declared inside the body of the program and are stored in RAM, thus may be changed on the fly. An example would be where you may want an input to output to perform one function in part of the program and another in a different part of the program.
Event triggering
The most common use of the I/O is to trigger events within a system:
- Inputs: to trigger events internal to the MDrive program.
- Outputs: to trigger events within a machine or system.
Input example:
The following program example shows an input used to trigger an internal event:
The following program will move the axis to an absolute position based upon the state of I/O 1 and will hold that position until the state changes.
In this example, the program will use a conditional branch (BR) to activate the event. Input-driven events may also use the Call Subroutine (CL) command in a similar fashion.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 |
S1=0,0,0 ‘setup io point ‘***program*** PG 100 ‘enter program mode at address 100 LB SU ‘label program to start on power on LB ba ‘label ba is a loop point ‘*** input event actions*** BR bb, I1=1 ‘conditional branch to bb if input 1=1 BR bc, I1=0 ‘conditional branch to ba if input 1=0 ‘*** input event 1*** LB bb ‘ create process bb MA 51200 ‘move to absolute position 51200 H0 ‘hold until motion ceases BR ba ‘loop to ba ‘*** input event 0*** LB bc ‘create process bb MA 0 ‘move to absolute position 0 H0 ‘hold until motion ceases BR ba ‘loop to ba ‘***end*** E PG |
Output event
The following program example shows an output used to trigger an external event. A real-world example may be that the MDrive performs and completes a task, when complete the program will activate an output to trigger an external process, such as executing a program in a second system MDrive.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 |
S1=0,0,0 ‘setup IO1 S2=16,0,0 ‘setup IO2 ‘***program*** PG 100 LB SU LB ba ‘label ba as return point MR 512000 H0 ‘***initiate external event*** O2=1 ‘set output 2 active ‘***wait for input to restart*** LB bb ‘ label bb as loop point BR bb, I1=0 ‘loop to bb, input 1 inactive BR bc, I1=1 ‘branch to bc, input 1 active ‘***restart program on input event*** LB bc ‘label bc as clear O2 02=0 ‘set output 2 inactive BR ba ‘restart program E PG |
Using a Bank of I/O
The MDrive I/O can read inputs and write outputs as a group in Binary Coded Decimal (BCD).
The I/O may be connected as shown below. For purposes of example, we have used switches for inputs and LED’s for outputs. All are configured as general purpose, active when low, sinking.
For this example we will use two basic programs:
- Inputs: A program that will perform a specific move based on the input decimal value.
- Outputs: A program that will cause the outputs to operate as a binary up counter.
Move on BCD Input Example
The following application will move the motor to a variety of positions based upon a binary input to I/O 1-4. One of the things this application shows is one of the new Microstep Resolution settings that give the ability to set motion to occur in 0.001˚ increments. The program does a calculation after each move to show motor position in degrees. To make the web view shorter, the example below omits many repetitive branch routines for the various moves. See the full program to view.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119 120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138 139 140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 |
‘******Global Setup Parameters**** S1=0,0,0 ‘I1–4 set as GP,LOW Active, sinking S2=0,0,0 S3=0,0,0 S4=0,0,0 P=0 Ms=180 ‘Microstep Res to 0.001 deg/ustep ‘******Main Program********* PG 1 LB aa R1=Il ‘Set register 1 = inputs 4-1 BR z1,R1=0 ‘conditional branches based BR za,R1=1 ‘upon the value of IL BR zb,R1=2 BR zc,R1=3 BR zd,R1=4 BR ze,R1=5 BR zf,R1=6 BR zg,R1=7 BR zh,R1=8 BR zi,R1=9 BR zj,R1=10 BR zk,R1=11 BR zl,R1=12 BR zm,R1=13 BR zn,R1=14 BR zo,R1=15 BR aa ‘*******Program Motion Components******* LB z1 BR aa, P=0 ‘branch to main prog, position=0 MA 0 ‘index to abs. pos. 0 H ‘Suspend prog. until move completes CL zz ‘call the print position sub. BR aa ‘BR to main prog when complete LB za ‘same as above BR aa, P=36000 MA 36000 H CL zz BR aa LB zb BR aa, P=-36000 MA –36000 H CL zz BR aa LB zc BR aa, P=18000 MA 18000 H CL zz BR aa LB zd BR aa, P=-27000 MA –27000 H CL zz BR aa LB ze BR aa, P=9000 MA 9000 H CL zz BR aa LB zf BR aa, P=-9000 MA –9000 H CL zz BR aa LB zg BR aa, P=4500 MA 4500 H CL zz BR aa LB zh BR aa, P=-4500 MA –4500 H CL zz BR aa LB zi BR aa, P=3000 MA 3000 H CL zz BR aa LB zj BR aa, P=-3000 MA –3000 H CL zz BR aa LB zk BR aa, P=6000 MA 6000 H CL zz BR aa LB zl BR aa, P=-6000 MA –6000 H CL zz BR aa LB zm BR aa, P=7500 MA 7500 H CL zz BR aa LB zn BR aa, P=-7500 MA –7500 H CL zz BR aa LB zo BR aa, P=0 MA 0 H CL zz BR aa ‘****Print Position Subroutine**** LB zz R2=P/100 ‘set register 2 to position/100, ‘this will display degrees as the unit ‘of measure for motor position PR “Position Selected = “,R1 PR “Absolute Position (Degrees) = “,R2 RT E PG |
Binary up counter – BCD output example
The following program example shows the use of the lower output bank as a binary up-counter. IO1 – IO4 are setup as general purpose outputs, active when HIGH, sinking. The main program will set the outputs, store the decimal equivalent of the outputs, and index the motor a multiple of the output state. Once complete it will increment the register and repeat until the value of the register =15 (binary 1111). It will then clear the register, set the outputs to 0, and restart the process.
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 |
‘***Global Setup Parameters*** S1=16,1,0 ‘O1–4 Set as GP, High Active, Sinking S2=16,1,0 S3=16,1,0 S4=16,1,0 ‘***Main Program*** PG 1 LB aa CL xx, R1<15 ‘Call sub xx R1 less than 15 CL zz, R1=15 ‘Call sub zz R1 equal 15 BR aa ‘***Subroutines*** LB xx ‘subroutine increments R1, moves motor R1=R1+1 ‘multiple of R1 value Ol=R1 ‘sets output group to R1 H 1000 ‘hold program execution for 1 sec. MR R1*100000 ‘move relative R1 x 100000 steps H ‘hold until motion completes RT ‘return from subroutine LB zz ‘subroutine to resets R1 to 0 R1=0 ‘and restart process RT ‘return from subroutine E PG |
Resource files
When it comes to your form, fit and function requirements, don’t settle. Get precisely what you need working with us. We know motion.
Contact us with any questions about how we can help you with your motion application or for assistance with your SEM products.
Browse our resource section and find the most useful tools and documents for all our products.