Application note

Initial Serial Connection

Home > Resources > Application notes > Initial Serial Connection

Description

This tutorial will guide you through the initial process of connecting to your SEM serial product using the Motion Control Programmer (MCP) application, part of the Software Suite.

This process is the same for any product communicating over a serial datalink, or using MCode over Ethernet.

Applicable

  • Lexium MDrive

Requirements

  • Download and install the Lexium MDrive Software Suite
  • RS-422/485 communications adapter drivers installed and connected between host PC and SEM product.
  • Product is in a powered ON state.
Lexium Software Suite
Download

User interface software for all Lexium MDrive products.

Details

Install the Lexium MDrive Motion Control Programmer

  1. Click the button labeled “Install Motion Control Interface” (1).
    Install MCP
  2. Follow the prompt dialogs to install the application. When completed the button text will change to “Launch Lexium MDrive Motion Control Interface” (2). Click to launch the application.
    Install MCP
  3. The program will open.
  4. Click the tab labeled “Terminal1” (3) to activate the terminal window. Direct (immediate mode) communications will be performed using this tab and the status bar (4).
    Install MCP

Establish Communications

Communications Configuration

  1. With the tab labeled “Terminal1” active, double-click the COM port: BAUD rate (1:9600) field of the status bar (1). This will open the Terminal Preferences dialog. Note: The Terminal Preferences dialog may also be opened using the menu items Edit > Preferences > Terminal Settings.
  2. Select the COM port (2) your communications adapter is installed on.
  3. Verify that the Lexium MDrive default BAUD rate, 9600 kbps, is selected (3)
  4. Click the button labeled “Set” (4). The dialog will close.
  5. Double-click “Port Closed” (5) on the status bar, it should change to “Port Open” (6)
  6. Key in the sequence, CTRL+C (7) or cycle power on the Lexium MDrive.
  7. You should see the sign-on message “Copyright © 2010-2014 Schneider Electric Motion USA” (8) appear within the Terminal1 tab, along with the “>” prompt. This signifies that the device is communicating. You may now send commands and programs to the Lexium MDrive Motion Control device.

Resource files

When it comes to your form, fit and function requirements, don’t settle. Get precisely what you need working with us. We know motion.

Contact us with any questions about how we can help you with your motion application or for assistance with your SEM products.

Browse our resource section and find the most useful tools and documents for all our products.