Application note
Configuring MDrive I/O: Sourcing I/O
Home > Resources > Application notes > Configuring MDrive I/O: Sourcing I/O
Description
A sourcing device provides the power or a positive potential to an I/O point. Sourcing devices ‘push’ the current through the load. Other terms used to describe sourcing devices include PNP, Open Emitter, Normally Low, and IEC Positive Logic.
Note that sourcing outputs are only available on Motion Control devices equipped with Plus2 expanded features.
For this part of the tutorial we will use the same hardware configuration examples as was used in the Connecting Power and I/O tutorial to show the configuration of I/O points to various I/O uses.
Applicable
- MDrive Linear Actuator
- MDrive Plus
- MForce
Requirements
- DC power supply
- Optional: +5 to +34 VDC Auxiliary supply
- +5 to +24 VDC I/O supply (if using sourcing outputs).
- Input and/or output devices
- Cabling: 22 AWG shielded twisted pairs for I/O, Shielded twisted pair for power, AWG determined by length and current.
Details
PNP Input
In this example case we will assume that we need a PNP Sensor connected to an input to trigger events within an MDrive program. Thus we will configure I/O point 1 as a General Input which will activate when HIGH.
The command:
1 |
S1=0,1,1 |
will set I/O1 to function as we desire:
- S1=: setup I/O 1
- 0: General purpose input function
- 1: Active when HIGH
- 1: Sourcing input type
Switch Input
In this example case we need a Start switch to execute an MDrive program.
The commands:
1 |
S1=4,1,1 |
will set I/O 1 to function as we desire:
- S1=: setup I/O 1
- 4: G0 input function
- 1: Active when HIGH
- 1: Sourcing input type
Inductive Load Output
In this example case we will configure a sourcing output. When active, the output will energize a solenoid which in turn will activate another system process based upon an event inside an MDrive program.
The command:
1 |
S12=16,1,1 |
will set I/O 12 to function as we desire:
- S12=: setup I/O 12
- 16: FGeneral purpose output function
- 1: Active when HIGH
- 0: Sourcing output type
Resource files
When it comes to your form, fit and function requirements, don’t settle. Get precisely what you need working with us. We know motion.
Contact us with any questions about how we can help you with your motion application or for assistance with your SEM products.
Browse our resource section and find the most useful tools and documents for all our products.