Accessory Types: Prototype Cable

PD04-MF34-FL3 Prototype development cable

To speed your test/development, this cable  is pre-wired with 4-pin locking wire crimp connector mate, 3.0 m / 10.0 feet long to connect a motor to the MForce PowerDrive.

PD04-MF17-FL3 Prototype development cable

To speed your test/development, this cable  is pre-wired with 4-pin locking wire crimp connector mate, 3.0 m / 10.0 feet long to connect a motor to the MForce MicroDrive.