Accessory Types: Protection Module

DPM75 Drive protection module

The function of the DPM75 Drive Protection Module is to limit the surge current and voltage to a safe level when DC input power is switched on and off to a motor drive. This provides the added protection necessary for reliable motor drive operation when switching the DC power, instead of the recommended AC power …

DPM75 Drive protection module Read More »