Menu

Accessory Types: Mounting Hardware

HY462-CN021 21 Pin Right Angle Connector

HY462-CN021 21 pin right angle connector for the IB462He PCB-mount driver module mounts to the user’s PCB prior to soldering to provide an easy pluggable interface for the driver module.

PR-22-G1 23 Pin Receptacle

The PR-22-G1 receptacle consists of a removable plastic carrier frame with 23 pin sockets for the IM483H Plus or IM805 Plus PCB-mount microstepping driver module. The assembly is seated into the PCB prior to soldering, then the plastic carrier frame is removed and discarded.

Do NOT follow this link or you will be banned from the site!