Menu

Accessory Types: Starter Kit

XIM483H-DK1/ XIM805H-DK1 Developer’s Kit

XIM483H-DK1/ XIM805H-DK1 Developer’s Kit includes everything needed to begin developing applications using the IM483H plus or IM805H Plus microstepping PCB-mount driver module. Includes an INT-483H/INT-805H interface board and an HFC-22 Heat Sink/Fan/Clip Assembly.

LMM-KIT2 CANopen single axis starter kit

Starter kit contains everything needed to begin developing applications for the Lexium Motion Module CANopen. Kit includes: LMM-15-A 1.5 Amp Lexium Motion Module CANopen LMM-INT1-A development board DC power supply MD-CC501-000 communications converter NEMA 17 (42 mm) rotary motor Single-end encoder

LMM-KIT1 Programmable Motion single axis starter kit

Starter kit contains everything needed to begin developing applications for the Lexium Motion Module Programmable Motion Control. Kit includes: LMM-15-M 1.5 Amp Lexium Motion Module Programmable Motion Control LMM-INT1-M development board DC power supply MD-CC404-000 communications converter NEMA 17 (42 mm) rotary motor Single-end encoder

Do NOT follow this link or you will be banned from the site!