Menu

Accessory Types: Backup Battery pack

Absolute Encoder Backup Battery pack

For Lexium MDrive Products with Absolute Encoder The ICP0531 Encoder Back-up Battery Pack will provide back-up power for the Lexium MDrive Absolute Encoder circuitry, retaining and updating the position data for a period of up to five (5) years. The battery pack requires three (3) Energizer L91 1.5V AA Lithium batteries. Battery voltage level monitoring The ICP0531 …

Absolute Encoder Backup Battery pack Read More »

Do NOT follow this link or you will be banned from the site!