UL recognition

MDrivePlus 34AC
certification

• Application information and
  & conditions of acceptability

• UL recognized - US standard
  UL508C

• UL recognized - Canadian national
   standard C22.2 No. 14-05

REACH compliance

Registration, Evaluation, Authorization and Restriction of Chemicals (REACH). REACH is a European Community Regulation on chemicals and their safe use (EC 1907/2006).

• REACH Compliance for
  Lexium MDrive Products

RoHS compliance

The RoHS (Restriction of Hazardous Substances) European directive was implemented on July, 1st, 2006. This directive - which requires the elimination of lead, mercury, cadmium, hexavalent chromium and polybrominated biphenyls, polybrominated diphenyl ether flame retardants in certain Electrical and Electronic Equipment put on sale in Europe. Schneider Electric Motion USA is in full compliance with the directive.

• Letter of conformity
  (updated 02/22/2012)

 

 

 

 

ISO certification

In December 2010 Schneider Electric Motion USA was certified ISO 9001 and ISO 14001. Below are the documents relavent to this certification.

Download

EtherNet/IP conformance tested

All Schneider Electric Motion Ethernet products are conformance tested by the ODVA and meet applicable standards.
  > Download Conformance Certificate

CE declarations of conformity

The products listed conform to the directives and standards of CE (Certified Europe)
For CE test environment details, contact an Application Engineer tel: +01-860-295-6102
 
Lexium MDrive Products
All NEMA sizes
  • Lexium MDrive Motion Control
  • Lexium MDrive Pulse/direction
 
MDrivePlus and Linear Actuators

MDrive14Plus
  • MDrive14Plus Motion Control
  • MDrive14Plus Microstepping

MDrive17Plus
  • MDrive17Plus Microstepping
  • MDrive17Plus Motion Control
  • MDrive17Plus Speed Control

MDrive23Plus
  • MDrive23Plus Microstepping
  • MDrive23Plus Motion Control
  • MDrive23Plus Speed Control
  • MDrive23Plus Motion Control Ethernet

MDrive34Plus
  • MDrive34Plus Microstepping
  • MDrive34Plus Motion Control
  • MDrive34Plus Speed Control

MDrivePlus 34AC
  • MDrivePlus 34AC Microstepping
  • MDrivePlus 34AC Motion Control

 
 
 
 
Panel mounted drivers

MicroLYNX
  • MicroLYNX -4/7

IM483
  • IM483

IM805
  • IM805

 
 
 
MDrive Hybrid

MDrive Hybrid 17
  • MDrive Hybrid 17 Motion Control

MDrive Hybrid 23
  • MDrive Hybrid 23 Step • Torque • Speed
  • MDrive Hybrid 23 Motion Control
  • MDrive Hybrid 23 Motion Control Ethernet

MDrive Hybrid 34
  • MDrive Hybrid 34 Step • Torque • Speed

MDrive Hybrid 34AC
  • MDrive Hybrid 34AC Step • Torque •
    Speed
  • MDrive Hybrid 34AC Motion Control

 
 
 
 
MForce

MicroDrive
  • Microstepping MicroDrive
  • Motion Control MicroDrive

PowerDrive
  • Microstepping PowerDrive
  • Motion Control PowerDrive

 
 
 
 
PCB mounted drivers

IM481H Plus
  • IM481H Plus

IM483H & IM805H Plus
  • IM483H Plus
  • IM805H Plus