We offer 1.8° enhanced hybrid stepper motors which have higher torque output than conventional hybrid stepper motors. These high performance motors, available in several NEMA sizes and lengths, are the perfect match for our stepper motor drivers.
1.8° hybrid stepper motors
NEMA 14
Phase current: 0.75 Amps
Holding torque: 10 oz-in (7 N-cm)
NEMA 17
Phase current: 1.5 Amps
Holding torque: 32 to 75 oz-in (23 to 53 N-cm)
NEMA 23
Phase current: 2.4, 3.0 & 6.0 Amps
Holding torque: 90 to 257 oz-in (64 to 181 N-cm)
NEMA 34
Phase current: 6.3 Amps
Holding torque: 419 to 1303 oz-in (296 to 920 N-cm)