Products

 

 

 

 

Exhibition

See MDrive products in action at

Medical Design & Manufacturing East
Jun 18 - 20, 2013
Booth # 3745
Pennsylvania Convention Center,
Philadelphia, Pennsylvania
Learn more

 

 

 

 


Panel mounted microstepping drivers


These discrete microstepping drivers deliver high performance in incompact packages that include up to
14 selectable resolutions and built-in protection.


 

 


Products



IM483 panel mounted driver

>  +12 to +48 VDC, 3.0 amps RMS (4.0 amps peak)   IM483
>  +24 to +75 VDC, 5.0 amps RMS (7.0 amps peak)   IM805