• MDrive/MForce
  • MDrive Hybrid

  • Motion Control
  • Step / direction
  • EtherNet/IP
  • CANopen
  • Speed Control
 

SEM Terminal

For use with all Lexium MDrive MDrive/MForce/MicroLYNX products.

SEM Terminal is the next generation of the IMS Terminal program enhanced with advanced features and functionality.

Compatible with Windows 7 and Wimdows 8 64-bit operating systems.

Download SEM Terminal
Version 5.0.2.0
Release Date: November, 22, 2013
File Size: 7.9 MB
Requirements: Windows XP Service Pack 3 or Higher

 

 
 

 

TCP/IP configuration tool

For use with MDrivePlus units with an Ethernet communication interface. Required to configure the IP address and subnet mask. Includes a terminal emulator for MCode/TCP, a PDU entry dialog for sending MODBUS/TCP commands and Assembly object mapping tool for EtherNet/IP.

Screenshots
> Configuration
(MCode/TCP)
> SEM Port (MCode/TCP)
> MODBUS Motion (MODBUS/TCP)
> MODBUS Manual Entry (MODBUS/TCP)

Download Administrator Install
Version 1.0.0.7
Release Date:June 13, 20113
Requirements: Windows XP Service Pack 2 or Higher
TFTP Server 32-bit
TFTP Server 64-bit

TFTP Server, installation is only required if you are going to upgrade the ethernet controller firmware in your device. Not required to ugrade main system firmware.

Instructions on performing this upgrade are located HERE.

 

 

 

 

SPI Motor Interface

For use with MDrivePlus and MForce Step / direction units with an SPI communication interface.

Resources
> Installation and usage tutorials

Screenshots
> Motion settings

> I/O settings
> Part & Serial number
> Upgrader utility

Download SPI Motor Interface
Version 3.1.70 - Change summary
Release Date: October 21, 2011
File Size: 3.5 MB
Requirements: Windows XP Service Pack 2 or Higher

 

 

 

TCP/IP configuration tool

For use with MDrivePlus EtherNet/IP units Required to configure the IP address and subnet mask. Includes a utility for mapping the Assembly object..

Screenshots
> Configuration

> Assembly object mapping

Download Administrator Install
Version 1.0.0.6
Release Date:August 24, 2012
Requirements: Windows XP Service Pack 2 or Higher
TFTP Server 32-bit
TFTP Server 64-bit

TFTP Server, installation is only required if you are going to upgrade the ethernet controller firmware in your device. Not required to ugrade main system firmware.

Instructions on performing this upgrade are located HERE.

NOTE: The 1.0.0.6 release is in supprt of PLCs that do not have explicit messaging capabilites. Firmware version 1.2.0.5 is also required to use this functionality

 

 
 

CANopen Tester

For use with MDrivePlus and MForce CANopen units with a CANopen communication interface.

Use of this tool requires the MD-CC500-000 USB to CANopen converter cable.

Download CANopen Tester

Version 3.51.0 - Change summary
Release Date: July 29, 2013
File Size: 9.0 MB
Requirements: Windows XP Service Pack 2 or Higher

CANopen Electronic Datasheet (EDS)

 

 
 

SPI Motor Interface

For use with MDrivePlus Speed Control units with an SPI communication interface.

Screenshots
> Analog settings

> Motion settings

> I/O settings
> Part & Serial number
> Upgrader utility

Download SPI Motor Interface
Version 3.1.68 - Change summary
Release Date: October 19, 2010
File Size: 3.5 MB
Requirements: Windows XP Service Pack 2 or Higher

 

 

  • Motion Control
  • Step • Torque • Speed
  • EtherNet/IP
  • CANopen
 

SEM Terminal ***BETA***

For use with all Lexium MDrive MDrive/MForce/MicroLYNX products.

SEM Terminal is the next generation of the IMS Terminal program enhanced with advanced features and functionality.

Compatible with Windows 7 and Wimdows 8 64-bit operating systems.

Please note that this is a beta version of the SEM Terminal which is still undergoing final testing before its official release. The oftware is provided on an
“as is” basis.

Download SEM Terminal Beta
Version 905.0.0.36
Release Date: November, 11, 2013
File Size: 7.9 MB
Requirements: Windows XP Service Pack 3 or Higher

 

 
 

IMS Terminal

For use with MDrive Hybrid units with an RS-422/485 or Ethernet communication interface.

Select the ASI radio button in the "Device" frame of the "Comm Settings" tab of the Preferences dialog.

Resources
> Installation and usage tutorials

Screenshots
> Main screen

> Comm settings (RS-422/485)
> Comm Settings (Ethernet)
> Function Key setup

Download IMS Terminal
Version 4.4.6 - Change summary
Release Date: June, 20, 2012
File Size: 7.9 MB
Requirements: Windows XP Service Pack 2 or Higher
If using Microsoft Windows 7 64-bit or Windows 8, please use the SEM Terminal Beta software above.

 

 

 

TCP/IP configuration tool

For use with MDrive Hybrid units with an Ethernet communication interface. Required to configure the IP address and subnet mask. Includes a terminal emulator for MCode/TCP use and a PDU entry dialog for sending MODBUS/TCP commands.

Screenshots
> Configuration
(MCode/TCP)
> SEM Port (MCode/TCP)
> MODBUS Motion (MODBUS/TCP)
> MODBUS Manual Entry (MODBUS/TCP)

Download Administrator Install
Version 1.0.0.7
Release Date:June 13, 20113
Requirements: Windows XP Service Pack 2 or Higher
TFTP Server 32-bit
TFTP Server 64-bit

TFTP Server, installation is only required if you are going to upgrade the ethernet controller firmware in your device. Not required to ugrade main system firmware.

Instructions on performing this upgrade are located HERE.

   

 

 

 

 

MDrive Hybrid Configuration Utility

For use with MDrive Hybrid Step • Torque • Speed units with an RS-422/485 communication interface. Required to configure the mode of operation.

Screenshots
> Hybrid Config. Utility main screen

> Hybrid Setup
> Hybrid Operation
> Hybrid Status
> Hybrid Calibration

> Analog settings
> Communication settings
> I/O settings
> Motion settings
> Additional Motion Settings
> Read/Restore defaults

Download Administrator Install
Download Single-user Install
Web-based installer

Version 1.0.0.7
Release Date: 28 July 2012 - Change summary
File Size: varies with download method selected

Requirements: Windows XP Service Pack 2 or Higher
, Windows installer 3.1+, ,NET Framework 3.5+.

NOTE: If the Utility is already installed on your system using the web-based install it will automatically update if your system is connected to the internet.

 

 

 

TCP/IP configuration tool

For use with MDrive Hybrid EtherNet/IP units Required to configure the IP address and subnet mask. Includes a utility for mapping the Assembly object..

Screenshots
> Configuration

> Assembly object mapping

Download Administrator Install
Version 1.0.0.6
Release Date:August 24, 2012
Requirements: Windows XP Service Pack 2 or Higher
TFTP Server 32-bit
TFTP Server 64-bit

TFTP Server, installation is only required if you are going to upgrade the ethernet controller firmware in your device. Not required to ugrade main system firmware.

Instructions on performing this upgrade are located HERE.

NOTE: The 1.0.0.6 release is in supprt of PLCs that do not have explicit messaging capabilites. Firmware version 1.2.0.5 is also required to use this functionality

 

 
 

CANopen Tester

For use with MDrive Hybrid CANopen devices.

Use of this tool requires the MD-CC500-000 USB to CANopen converter cable.

Download CANopen Tester

Version 3.50.0 - Change summary
Release Date: July 24, 2012
File Size: 9.0 MB
Requirements: Windows XP Service Pack 2 or Higher

Hybrid CANopen Electronic Datasheet (EDS)